Skip to main content

Boost your property's value and cut energy costs with a heat pump

Installing a heat pump can increase your property’s value by improving energy efficiency, lowering running costs, and boosting its Energy Performance Certificate (EPC) rating. Across Europe, homes with sustainable heating systems are more attractive to buyers and often command higher prices. This article explains how heat pumps enhance efficiency, why EPC ratings matter, and the impact on resale value. Beyond energy savings, a heat pump is a future-proof investment that improves comfort, cuts bills, and positions your home for stronger market appeal.

Efficient, sustainable – and profitable

A heat pump uses up to 80% of its energy from renewable air or ground heat. Powered by a fraction of electricity, it can deliver three to four times more energy than it consumes – resulting in a 300% to 400% efficiency gain compared to traditional fossil fuel systems.

For homeowners, that means lower operating costs, reduced carbon emissions, and a clear advantage in the property market.

Energy efficiency is fuelling buyer decisions

Across Europe, energy performance has become a key driver in the buying and selling process. With Energy Performance Certificates (EPCs) now mandatory under the Energy Performance of Buildings Directive (EPBD), a home’s energy rating plays a direct role in determining its market value.

EPCs rate homes from A to G (most to least efficient), based on factors such as insulation, heating systems and overall energy use. Installing a heat pump is a proven way to improve a home’s EPC rating – often by one or more classes – depending on the existing heating setup and whether radiators or underfloor emitters are also upgraded.

The market premium for energy efficiency

Our research across Western Europe, covering Germany, France, Italy, Spain, Belgium, the Netherlands and the UK, shows that improving a property’s energy rating through interventions like heat pump installation consistently leads to higher sale prices.

  • Germany: A 100 kWh/m² annual reduction in energy use can boost home prices by an average of 6.3% in urban areas.
  • France: Upgrading from EPC class D to A or B increases value by 6% to 14%.
  • Spain: Homes rated A–C sell for an average 7.5% more than those rated D–G.
  • Italy: Moving from class E to D can yield a 5%–6% gain, while a shift from G to D can raise property value by 14%–18%.

Buyers today are looking for homes that deliver long-term value—not just in resale terms, but in energy savings and environmental impact.

Future-proof your home – and its value

As the EU pushes forward with tighter emissions legislation and energy performance standards, the case for heat pumps is only getting stronger. Homes that meet higher EPC standards are not only cheaper to run—they’re more compliant, more marketable, and more resilient to the policy changes ahead.

Conclusion

Heat pumps are a high-impact, low-carbon upgrade that deliver measurable returns—both financially and environmentally. They improve your home's EPC rating, lower ongoing costs, and increase its market appeal at a time when energy performance is under growing scrutiny.

Key takeaways

  • Heat pumps can increase property value by improving energy efficiency and EPC ratings.
  • The value of energy-efficient homes can increase up to 18% in some European markets.
  • Installing a heat pump is a long-term investment, combining sustainability with financial returns.
  • Homes with heat pumps are better positioned for the future, combining compliance, comfort and resale appeal.

For detailed figures, regional comparisons, and the full research methodology, download our whitepaper in English.

More reasons to choose a heat pump