Skip to main content

Our certified heat pump installers are ready to deliver

So you've decided a heat pump is the future-proof way of heating your home. Now you're looking for a heat pump installer near you, to discuss your project and get a price quote. Daikin is here to help. Simply fill in our form and a certified installer will be in touch.

STEP 1: FILL IN THE FORM

Filling in the form helps us to connect you to a certified installer for your new heat pump.

Please include important details about your project:

  • Tell us a bit about your current central heating installation.
  • Explain what you're planning. Are you simply replacing your central heating installation? Planning a renovation? Or building a new home?
  • Maybe you've spotted a Daikin product that looks right for you. Feel free to let us know which product interests you.

With this information, we can match you to the perfect heat pump installer for your project.

STEP 2: WE MATCH YOU TO A CERTIFIED DAIKIN HEAT PUMP INSTALLER NEAR YOU

Great! By filling in the form, you've taken the first step to heating and cooling your house with a heat pump. Here's what happens next.

First, we match you to a certified Daikin heat pump installer near you. All our installers have experience installing Daikin products.

We select a heat pump installer based on these criteria:

  • They are an experienced certified installer of the product you have in mind
  • They speak your language
  • They are available for new projects
  • They are close to you
  • They have the best feedback score

Please allow a few days for us to match you to the heat pump installer.

One or two working days after you fill in the form, we'll email you the name of the best installer for your project.

STEP 3: THE INSTALLER CONTACTS YOU

A few days after you receive your installer's name, they will contact you to arrange a site visit. (Of course, if you prefer, you can contact the installer yourself, once you receive their details.)

STEP 4: THE SITE VISIT

A site visit allows the heat pump installer to understand your needs and the possibilities of your home. With that information, we can propose the best product for your needs.

The installer will check:

The energy efficiency of your house. What materials are used in your house? How well is it insulated? What type of glazing do you have?

Your existing central heating system and needs. How large is your house? Which rooms need cooling, heating, ventilation or air purifiers? How many heating elements (like radiators) do you have in your house? How powerful are they?

Your lifestyle. How many people live under your roof? How often are you at home? What is your preferred temperature inside the room? How much hot water do you use?

Practical information for the heat pump installation. The certified installer will check where to install outdoor and indoor units and where to lay the piping.

If you have questions, the site visit is the best time to ask them. Some of the questions you might want to ask are:

  • Is a heat pump right for me? Your installer can help you, by discussing your needs and expectations, your existing setup and also the financial implications, to decide if a heat pump is the right solution for you.
  • Which type of heat pump is most suitable for my home? The installer can explain the different types of heat pump and their costs and installation procedures, to help find out which is best for you. Typically these might include a high- or low-temperature air-to-water heat pump, a ground source heat pump or a hybrid system.
  • Do I need any additional building works for a heat pump to work efficiently? At the visit, your installer may suggest some steps you can take to maximise your heat pump's efficiency, especially if you live in an older building. They could include loft or wall insulation, draughtproofing or double glazing.
  • What capacity heat pump do I need? To recommend the right capacity heat pump for your needs, your installer will consider the size of the property, along with several other factors including its age and its energy efficiency. This will ensure your heat pump provides precisely what your home needs, no more and no less.

STEP 5: THE PRICE QUOTE

Shortly after the site visit, the heat pump installer will send you a quote for your desired solution.

In the offer you will find:

  • The price of the Daikin products: the price of the outdoor unit, the indoor unit and the controller
  • The price for other materials needed for the job: the piping and any other parts necessary to install your heat pump
  • The price of installation: the work that goes into installing your heat pump

Additionally, the installer might offer you a maintenance contract

Good to know: you might receive subsidies or tax benefits.

In most countries, heat pumps are eligible for subsidies or tax benefits. Check local incentives that apply after you get your price quote. It would be a pity to miss out on these.

STEP 6: THE HEAT PUMP INSTALLATION

Once you accept the quote, you can count down to the day we install your new heat pump.

Tip: Order your heat pump well in advance. Particularly as winter nears, our certified installers can be very busy. The installation of your heat pump itself is quick: it usually takes just one or two days to install your heat pump and switch it on.

These are the steps your certified installer will typically take to install the outdoor unit of your heat pump system:

  • Choose the best place: the installer will take into account how strong the surface is and how much space there is around the unit
  • Place the unit: it must be securely fastened on a completely level surface, ideally on blocks, with space at the top for maintenance
  • Install the drain: a drain plug allows the installer to drain the outdoor unit
  • Widen the end of the pipes: the end of the piping is cut, deburred and widened
  • Fix the refrigerant pipes: union nuts are used to attach the widened sections of the pipes
  • Check for gas leaks: once the pipes are connected, the installer vents the unit and checks for gas leaks
  • Fill with coolant: in Daikin heat pumps this is usually the refrigerant R-32, which is filled in liquid state through the gas pipe
  • Connect the cooling pipes: the installer uses a special pipe bender and is careful to make sure no moisture or dust gets into the pipe
  • Electrical wiring: the electricity is connected and an earth leakage detector and circuit breaker are fitted
  • Trial run and testing: the installer measures the supply voltage and tests the system in both cooling and heating mode

STEP 7: YOUR HEAT PUMP IS READY TO GO

Now you can enjoy optimal indoor temperatures all year round, plus support from Daikin whenever you need it.

Congratulations, you are now a heat pump owner! You no longer need fossil fuels to heat your home. You are now part of the future of heating.

Your journey with Daikin doesn’t end there, however. We’re here to support you throughout the lifecycle of your heat pump, with our:

Stand By Me platform: Stand by Me is our easy-to-access aftercare platform. Simply click the link to register your product, and you’ll be able to see information about your product and the services that are available to extend its lifetime, all in one place.

By registering on the platform, you’ll get six months’ extended warranty free of charge. You’ll be able to explore our maintenance packages, to make sure your product gets the best care. You’ll even get handy reminders when your annual maintenance visit is due.

Onecta app: Get complete control over your heating and cooling systems – wherever you are, and in whatever way works for you – with our Onecta app.

With Onecta, you can set temperature schedules, change the operation mode, and review your energy consumption with an easy-to-use app on your phone – or via your voice-activated Alexa or Google Home assistants. You can even control multiple rooms in several homes or monitor the outdoor air quality and pollen levels. All you need to do is install the app, sharing access with your family and friends if you wish, and you’re good to go.

Download Onecta here.

Warranty packages: The quality of our products is second to none, but in the unlikely event that a problem does occur, you don’t need to worry. All our domestic products come with a two-year guarantee as standard.

If you register your product on Stand By Me within the specified time period, we’ll give you an extra six months’ warranty on top for free.

Our additional warranty packages cover your devices for up to 10 years, so you don't need to worry about anything going wrong over the longer term. If it does, we'll take care of it for you.

So you can relax and enjoy complete peace of mind that any technical issues will be covered. How's that for service?

Fill in the form now and let us connect you to the right installer for your new heat pump

Daikin works with trusted certified installers close to you. However, we're always available to answer your questions. Don't hesitate to contact us if you would like more information or help.