Skip to main content

Reduce your energy bill with air-to-air heat pumps

What is an air-to-air heat pump?

Let's get you familiar with our air-to-air technology.

Jump to this topic on this page

How does it work?

Find out how our air-to-air heat pumps work, from for 1 to or multiple rooms at a time.

Jump to this topic on this page

How much can I save?

Tired of high energy bills? Calculate how much a heat pump can save.

Jump to this topic on this page

How does it interact with my heating system?

Learn how easily a heat pump combines with your existing heating system.

Jump to this topic on this page

What is an air-to-air heat pump?

An air-to-air heat pump uses renewable energy to heat your home by extracting energy from the air outside and only using 20% electricity to do so - an exceptionally energy-efficient way to achieve the perfect temperature. No need to change your boiler or existing heating system, you can simply add it to your home.

To optimise its use and maximise your savings, we recommend installing the indoor unit in the most frequented room such as the living room, which can contain up to 70% of your energy consumption.

How does it work?

Pair: To heat one room, a single split system connects one indoor unit to one outdoor unit. Choose any type of indoor unit that fits your room the best. Adding an air-to-air system in one room e.g. the living room, will already reduce your energy consumption significantly compared to electric or combustion heating.

Multi: To heat up to 5 rooms, one outdoor unit can be connected to up to 5 different indoor units. The temperature and settings for each room can be controlled independently.

Multi+: To provide hot water and heat up to 3 rooms, the Multi+ outdoor unit is an all-in-one system ideal for houses of max. 80m².

Do you want deepdive into the details of the air conditioning process?

Pair

Multi

Multi+

How much can I save?

With efficiencies up to A+++ in heating, an air-to-air heat pump will save on your energy consumption and provide comfort all year long.

How does it interact with my actual heating system?

Actually, they complement each other very well. In spring and autumn, you can simply turn down the radiators or room thermostat. The air-to-air heat pump will be perfectly capable to cover the full demand.

In the heart of winter, you can open the radiators and have them work complementary with your air-to-air heat pump, as they will act as a secondary heat source when needed.

Your dealer will be able to inform you whether the heat pump can or cannot cover the full load.

Looking for a solution that fits your needs, home and budget?

Stylish examples of our air-to-air product range:

Click to view images in full size