Skip to main content

Learn how air purifiers neutralise cooking odours, what technologies are most effective, and how to choose the right model for a fresh kitchen

The most effective way to remove cooking odours is by using a high-quality air purifier with HEPA and activated carbon filters, combined with proper placement, regular maintenance, and good ventilation. It provides a practical alternative to temporary fixes like sprays, diffusers or candles. This guide explains how air purifiers work, where to place them, how to maintain and other habits to keep your kitchen odour-free.

Why cooking smells linger after meals

Cooking a delicious meal is a source of joy and creativity for many. From sizzling bacon to aromatic spices, cooking transforms our kitchens into sensory hotspots—but not all aromas are welcome after the meal is over. Persistent cooking smells like fried oil, garlic, and fish can linger in the air, seep into fabrics, and make your home feel less than fresh. Thankfully, modern air purifiers equipped with advanced filters, including activated carbon, offer an effective solution to get rid of stubborn kitchen odours.

Simply opening a window is often insufficient, especially in modern, airtight homes or during cold weather, when ventilation is limited. These smells cling stubbornly to surfaces, fabrics, and even your clothes, reducing comfort and freshness. This is where air purifiers come into play as a long-term, effective solution to keep kitchens smelling clean and inviting.

What causes persistent kitchen odours?

Scientifically, cooking odours are complex mixtures of chemicals that can be absorbed by porous materials in your home, making them difficult to eliminate with surface cleaning alone. Grease particles also play a significant role as they settle on walls, cabinets, and countertops, providing a medium for odours to linger.

Furthermore, kitchens with poor ventilation amplify this problem by trapping these compounds indoors, allowing them to accumulate and intensify. For example, have you ever woken up to, or even because of, the smell of last night’s delicious curry? Research shows that without proper air exchange or filtration, cooking smells can remain elevated for hours, causing unpleasant air quality.

How air purifiers remove cooking odours

Air purifiers work by drawing air through specialised filters that capture the particles and gases that are responsible for odours. Unlike sprays or candles, which mask smells temporarily, purifiers remove odour-causing molecules at their source, preventing the buildup that causes persistent kitchen smells. Some air purifiers, including Daikin’s range of solutions, use HEPA filters to trap fine particulates like smoke and grease as well as incorporate activated carbon filters that adsorb gaseous pollutants, effectively neutralising odours.

By integrating an air purifier into daily kitchen routines, homeowners can maintain fresher indoor air quality without constant manual intervention. Moreover, air purifiers can reduce allergens and airborne bacteria, offering an additional health benefit beyond odour control. This makes them a superior and sustainable choice compared to temporary masking agents.

What is a HEPA filter?

HEPA (High-Efficiency Particulate Air) filters are renowned for removing at least 99.97% of airborne particles as small as 0.3 microns, such as smoke, dust, and pollen. They work by mechanically trapping solid particles through dense fibre mats.

To effectively remove odours, HEPA filters are often paired with activated carbon filters that adsorb and neutralise these gaseous pollutants through millions of porous surfaces. Regularly replacing filters is crucial—HEPA filters typically last six to 12 months—since clogged or saturated filters reduce purifier performance and can even allow odours to linger.

Daikin's range of air purifiers uses electrostatic HEPA filtration, a high-efficiency particulate air filter system that is designed to catch fine particles of dust. Research shows they remove more than 99% of particles between 0.1microns and 2.5 microns in size.

What is a deodorising filter?

Deodorising filters are highly porous materials that work by adsorption, trapping odour-causing gases in millions of tiny pores. This makes them exceptionally effective at neutralising cooking smells, smoke, and chemical fumes that HEPA filters cannot catch. The porous surface of deodorising filter provides a large area to bind with molecules, removing them from the air and preventing odours from resurfacing.

Cooking odours from garlic, spices, and fried foods, which often contain complex organic compounds, are particularly well-handled by carbon filtration. Regular maintenance ensures continuous odour control and maximises purifier effectiveness.

How to choose the best air purifier for your kitchen?

When choosing an air purifier for the kitchen, focus on the features that directly impact odour removal, performance, and long-term costs:

  • Filter combination: Choose a model with electrostatic HEPA filtration and activated carbon filters to tackle both airborne particles (smoke, grease) and odour-causing gases from cooking.
  • Clean Air Delivery Rate (CADR): CADR indicates how efficiently the purifier removes smoke and cooking smells. Kitchens benefit from higher CADR values, especially when cooking frequently or using strong spices.
  • Room size and coverage area: Ensure the purifier’s coverage matches the actual size of your kitchen. Undersized units struggle to remove odours effectively, even with high-quality filters.
  • Carbon filter capacity: Air purifiers designed for kitchens often feature larger or enhanced carbon filters, which are more effective at neutralising persistent cooking odours.
  • Filter lifespan and replacement costs: HEPA filters generally last longer than other filter types, making them more cost-effective over time. Daikin air purifiers feature a filter with a lifetime of up to 10 years.
  • Ease of maintenance: Opt for purifiers with easy-to-replace filters to ensure consistent performance and reduce ongoing hassle in busy kitchen environments.

Where to put your air purifier?

Proper placement of an air purifier can make the difference between barely noticeable results and a kitchen that feels truly fresh after cooking.

For best performance, position the unit close to the source of odours—roughly 90 cm to 1.5 m from the stove—so it can capture smoke, steam, and airborne grease before they spread. Placing it too close risks clogging filters with grease and heat damage, while placing it too far reduces its ability to intercept odours early.

Height also plays an important role. A placement height of around 1–1.5 m above the floor aligns well with the level where most cooking particles and vapours circulate. Larger freestanding units can be placed on the floor, but they must have unobstructed intake and exhaust areas.

Avoid tucking the purifier behind cabinets or in corners where “dead zones” can form, trapping odours instead of circulating air. Maintain at least 25–30 cm of clearance from walls or furniture, and if possible, leave up to 1.5 m of open space around the unit for optimal airflow.

In open-plan kitchens, place the purifier so it works in harmony with existing ventilation—near but not directly in front of extractor hoods, vents, or windows—allowing both systems to complement each other rather than compete. Portable units offer the flexibility to move closer to the cooking area during meal prep, while built-in systems connected to HVAC can cover larger spaces but require professional installation.

By respecting distance, height, and airflow synergy, you maximize the purifier’s efficiency and extend its filter life.

Cooking habits that reduce odour production

Certain cooking methods naturally produce fewer odours and can help minimise kitchen smells:

  • Steaming, boiling, and air frying release less pollutants compared to frying or grilling.
  • Using lids and splatter screens limits oil and grease particles from escaping into the air.
  • Indoor grills equipped with filters further reduce smoke production.
  • Prepping ingredients by drying or marinating can lower oil splatter and smoke generation.
  • Finally, prompt cleaning immediately after cooking prevents grease and food residues from accumulating, which would otherwise contribute to persistent odours.

Adopting these habits can significantly reduce the intensity and duration of cooking smells in your home.

Tech features that make odour control smarter

Smart air purifiers increasingly feature technology to enhance odour control.

Key features that improve odour control include:

  • Sensors that automatically adjust fan speed for efficient filtration
  • Timers and scheduling functions that allow higher performance during cooking and reduced operation afterwards.
  • Quiet modes allow operation during nighttime or in open-plan living spaces without disruption.

These tech features make managing kitchen odours more convenient, efficient, and tailored to daily life.

How to clean and maintain your air purifier?

Dirty or clogged filters reduce an air purifier’s ability to remove odours effectively. Creating a filter maintenance schedule based on manufacturer recommendations and usage frequency helps maintain optimal performance.

Regularly cleaning the purifier’s outer shell and intake vents also prevents dust buildup that can obstruct airflow.

Common mistakes like running the unit with old filters or placing it in obstructed areas can drastically reduce effectiveness.

Consistent maintenance ensures your purifier continues to provide fresh, clean air, making it a reliable tool against kitchen odours over time.

How to ensure whole-home air freshness beyond the kitchen?

Cooking odours have a way of travelling far beyond the stove. In modern open-plan homes, or through HVAC ducts, the smell of last night’s curry or fried fish can quietly infiltrate dining rooms, living spaces, and even bedrooms—embedding itself in fabrics like sofas, curtains, and bedding. This isn’t just a nuisance for your nose: once airborne particles settle into textiles, they can be far harder to remove.

Using zone-specific air purifiers in these spillover areas helps contain odours at their point of spread and stops them from becoming part of the home’s “background scent.” This also brings a measurable health benefit. Research shows portable air purifiers can reduce indoor fine particulate matter (PM₂.₅) by 22% to 92% depending on conditions, cutting exposure to harmful particles linked to asthma, allergies, and cardiovascular problems. In one Shanghai trial, PM₂.₅ levels dropped from 96.2 µg/m³ to 41.3 µg/m³—almost a 57% reduction—after installing air purifiers.

The stakes are high: the annual burden of disease caused indoor air pollution, including polluted outdoor air used to ventilate indoor spaces, is estimated to correspond to a loss of many healthy life years. When it comes to respiratory illnesses, improved filtration and ventilation are capable of halfing those affected. Even low-level exposure to pollutants like nitrogen dioxide (NO₂) can exacerbate chronic cough, wheezing, and breathlessness, particularly in older adults.

Extending purification beyond the kitchen creates a consistently fresh, clean-air environment throughout the home. It not only keeps rooms smelling neutral but also supports better breathing, healthier sleep, and overall well-being—making fresh air an everyday luxury, not just a mealtime consideration.

FAQs about kitchen air purification

Can an air purifier really eliminate all cooking odours?

Air purifiers can dramatically reduce cooking odours (around 94% in just 60 minutes), but complete elimination isn’t always possible. Performance depends on several key factors: the quality and capacity of the filters must match the kitchen’s size and odour intensity. A purifier with a Clean Air Delivery Rate (CADR) too low for the room will struggle, while higher Air Changes per Hour (ACH) rates—ideally 4–6 for kitchens—can clear air more quickly. Air changes per hour is simply the number of times all the air in a room is replaced with completely new air, in one hour. A value of ‘5’ air changes per hour means a room’s entire volume of air is replaced with new air five times in one hour.

Airflow patterns matter too: blocked placement or stagnant air reduces efficiency, whereas positioning the purifier to work with natural ventilation or extractor fans improves results. Maintenance is equally critical, as saturated carbon filters lose their ability to trap odours and can even re-release them. Finally, odour sensitivity is subjective—what smells “fresh” to one person may still be detectable to another. For persistent odours, a higher-capacity purifier, multiple units, or combined strategies with ventilation and cleaning will deliver the most noticeable improvement.

Do air purifiers work better than exhaust fans for removing cooking odours?

Yes—especially for lingering odours and airborne pollutants. While exhaust fans work by venting air outdoors, they can’t capture microscopic particles that cling to fabrics and surfaces. High-quality air purifiers, particularly those combining HEPA and deodorising filters, can remove up to 99.97% of airborne particles and adsorb odour-causing gases directly. Exhaust fans also lose effectiveness in sealed, energy-efficient homes where air exchange is limited, whereas purifiers continuously cycle and clean indoor air without heat loss.

Can I use essential oils in my air purifier?

Only if the purifier is explicitly designed for it—many are not. Adding oils to standard purifiers can clog filters, damage internal components, and even void the warranty. Instead, those seeking fragrance can use diffusers or purifiers with a dedicated aromatherapy compartment. Even then, it’s worth noting that essential oils mask odours rather than removing them, so they should be used as a complement, not a substitute, for proper filtration.

Final thoughts: fresh air after every meal

In summary, air purifiers tackle cooking odours at their source by filtering both particles and gaseous pollutants, ensuring kitchens stay fresh and inviting. Consistent use, regular maintenance, and complementary habits like proper ventilation and cleaning maximise their effectiveness. With the right purifier and care, it’s possible to enjoy flavourful meals without sacrificing the freshness of your home.

Key takeaways

  • Modern air purifiers equipped with advanced HEPA filters, including activated carbon, offer an effective solution to get rid of stubborn kitchen odours.
  • Unlike exhaust fans that simply vent air outside, air purifiers actively capture microscopic particles and odour-causing gases to keep indoor air consistently cleaner.
  • Placing the air purifier at a height of about 1 to 1.5 metres and keeping the airflow unobstructed is essential for capturing cooking odours and particles effectively.
  • Dirty or clogged filters reduce an air purifier’s ability to remove odours effectively.
  • Adopting certain cooking habits can significantly reduce the intensity and duration of cooking smells in your home.