Skip to main content

Your fridge and an air conditioner use the same technology, and understanding that connection shows why heat pumps are one of the most energy-efficient ways to heat a home

An air conditioner and a refrigerator both move heat rather than generate it, using the same cycle of refrigerant, compressor, and expansion valve. Because moving heat requires far less energy than creating it, a heat pump can deliver 3 to 4 units of thermal energy for every unit of electricity consumed. This article explains the shared science and shows how heat pumps are a cheaper and more sustainable way of heating and cooling your home